L-com Expands Line of AC/DC Control Line Lightning and Surge Protectors NORTH ANDOVER, MA - 2/22/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added a whole new series of single stage AC/DC control line lightning and surge protectors. The new products protect 8 individual single ended AC or DC control lines using grounding lugs to provide tie points for earth ground. They all feature removable screw terminal strips for easy installation. Lightning and surge protectors are necessary for many wired connectivity lines. They protect sensitive electrical equipment on either end of a cable from transient voltage, or spikes, which may be caused by lightning strikes and other factors. AC and DC control lines are used in a range of applications and are commonly found on measurement and control equipment, computers, motor controllers and industrial automation equipment. The new products from L-com complement the existing 3-stage protectors by offering a more economical option. L-com will carry weather resistant models for 12VAC, 24VAC, 48VAC and 5VDC lines. The AC protectors feature Metal Oxide Varistors (MOV), while the DC protectors feature uni-polar Transient Voltage Suppression (TVS) Diodes rated at 1500 Watts. "It is common for engineers to overlook their AC/DC control lines when they have more pressing projects," said Patrick Pesa, Product Manager. "But it is a big mistake to leave those lines in place without any sort of protection. L-com makes protecting those lines easy and, with these new products, more economical than ever." Please click here to download a high-resolution version of the image suitable for print publication. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |