To our valued customers: Please note that our warehouses and offices will be closed on Thursday, July 4th in observance of the holiday.
 
 

L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications

Monday, March 18, 2019

IRVINE, Calif. (March 19, 2019) - L-com, an Infinite Electronics brand, and a preferred manufacturer of wired and wireless connectivity products, has unveiled a new line of Category 7 cables that are ideal for 10GBASE-T, Cat7 to Cat6a, factory automation, outdoor industrial Ethernet and machine vision applications.

L-com’s new Category 7 cables are constructed with an overall braid shield around individually shielded twisted pairs (S/FTP) and feature a ruggedized, die-cast metal RJ45 connector on each end. The halogen-free, TPU cable used in these assemblies is 10 Gig Category 7-rated, oil and UV resistant, flame resistant and is suitable for industrial or outdoor environments. Additionally, these cables have excellent flex characteristics with a bend radius of 1.39 inches.

“Whether you are using this in a standard Ethernet or GigE application, these cables are perfect for rugged factory, industrial or outdoor applications,“ said Dustin Guttadauro, Product Manager.

With included optional parts, the metal RJ45 connectors on these cables can easily be modified into a horizontal or vertical GigE configuration for machine vision applications. This unified GigE bracket is easy to install and contains spacers for 2 mm and 4 mm, making the plug compatible with either of the common machine vision standards. These cables have a temperature range rating to +60°C and are offered in off-the-shelf lengths of 1, 2, 3, 5 and 10 meters.

L-com’s new Cat7 10 Gig cables are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Infinite Electronics is a leading global supplier of electronic components serving the urgent needs of engineers through a family of highly recognized and trusted brands.  Our portfolio brands are specialists within their respective product set, offering broad inventories of engineering-grade product, paired with expert technical support and same day shipping. Over 100,000 customers across a diverse set of markets rely upon Infinite Electronics to stock and reliably ship urgently needed products every day.

<!--[if gte mso 9]> <w:LsdException Locked=""false"" Pri