New 3.5 GHz 802.16e WiMAX Compatible Amplifiers Add 1 Watt Power to Wireless Transmissions NORTH ANDOVER, MA - 6/14/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has released two new wireless RF amplifiers designed to add 1 Watt of power to 3.5 GHz transmissions, typically used in 802.16e WiMAX wireless applications. The new amplifiers, which are available for export, military, licensed amateur radio and OEM component sales only, can add up to 30 dBm output power to 3.5 GHz antennas. The HA3501I-1000 is for indoor applications only, while the HA3501-1000 is designed for outdoor applications and comes with a DC injector, 12 VDC power supply, and mast mount kit. Worldwide Interoperability for Microwave Access (WiMAX) is an IP based wireless broadband access technology that provides performance similar to 802.11 and Wi-Fi networks but has the coverage and quality of service (QOS) of cellular networks. Standardized by IEEE 802.16, it is intended for wireless "metropolitan area networks". The new amplifiers suit these applications where a greater range or signal strength is desired. "HyperLink's brand amplifiers have been a mainstay in our industry for decades," said Patrick Pesa, Director of Product Development. "Now under the L-com brand, we are extending our already broad range of products to support cutting edge wireless applications." Due to FCC regulations, the new amplifiers are not offered for general sale within the USA (see FCC Part 15 and Part 97 Notice in L-com's Terms & Conditions). For FCC supported applications, the new amplifiers will be stocked in L-com's Florida distribution center for same-day shipments. To download a high-resolution version of the image suitable for print publication, please click this link: https://www.L-com.com/lcom_emails/2012/061412/HA5801-1000.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |