USB Panel-Mount PCB Connectors Added to L-com Lineup ![]() NORTH ANDOVER, MA - 11/07/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added panel-mount USB connectors with PCB solder tails. The new connectors, which come in either USB 2.0 Type A Female or USB 2.0 Type B Female, are being sold in packages of 10. PCB connectors normally just rest on the board and can’t be locked down. L-com’s unique design allows an easy and permanent method to provide stability by adding two flanges to the USB connectors. The new connectors mount with standard 4-40 screws and use 30 microinch gold plated contacts to insure many mating cycles. "It is important to provide USB solutions to a wide variety of applications since USB is so popular today," said Steve Smith, Product Manager. "We have already had success with PCB connectors for our field termination USB connectors, so it was a natural extension for us to offer PCB USB connectors as well." The new connectors are stocked in the USA for same-day shipment, and 2-D engineering drawings and 3-D CAD models are available for free download from L-com's website. For a high-resolution version of the image suitable for print publication, please click here: https://www.l-com.com/lcom_emails/2012/110712/uc_a_pmt.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |