Multi-user multiple-input multiple-output (MU-MIMO) is the next evolution of MIMO and is revolutionizing that way Wi-Fi routers operate. MU-MIMO allows routers to simultaneously send data to multiple devices. This is much more efficient than single-user multiple-input multiple-output (SU-MIMO) that many routers utilize. MU-MIMO allows all of your devices to simultaneously send and receive data from the router for multiple devices at the same time.
If you’re not excited about MU-MIMO yet, here are 5 reasons why you should be:
- MU-MIMO eliminates slow Wi-Fi speeds by making your router a super multi-tasker. Instead of sending little bits of information one at a time to each device, the router can now simultaneously transmit data to multiple wireless devices.
- MU-MIMO is great for video streaming and other high-bandwidth uses because it delivers a more dependable, faster Wi-Fi connection, there is a noticeable improvement in these data-demanding tasks.
- Not only do Wi-Fi networks get faster with MU-MIMO, they gain greater capacity. This means that home networks can service more Wi-Fi devices and public networks with many users will perform better.
- Even non-MIMO devices will experience improved performance. To fully utilize MU-MIMO’s benefits, devices must support the technology. But with MU-MIMO devices working faster, the router is free to communicate with other SU-MIMO devices.
- MU-MIMO costs less and is easier to implement than SU-MIMO. MU-MIMO doesn’t require multiple antennas or as much signal processing as SU-MIMO. It also uses a simpler standardized beamforming method that makes it easier for manufacturers to support.
As with everything, MU-MIMO does have some downfalls. For optimal performance, both the router and device must support MU-MIMO using 802.11ac on the 5GHz frequency. No more than four devices should be connected at one time, for full, optimal performance, and those devices should be stationary and not roaming. MU-MIMO also only improves the connection in one direction, from router to device, or the downlink, not the other way around. Still, MU-MIMO is slated to be a very impactful technology and potentially revolutionize the world of wireless networking.
View our wide range of in-stock MIMO antennas.