Imagine a wireless network with more reach, capacity and scalability than any other wireless network, including cellular. That network exists and it is called the On-Ramp Total Reach Network. On-Ramp created the first wireless network built from the ground up to power wide-area machine-to-machine communication. This network uses patented technology to achieve unprecedented reach, capacity and scalability.
On-Ramp’s innovative technology operates in unlicensed bands and utilizes weak signals, even if they are in high-noise environments or over long distances with immunity to high-interference. This process produces groundbreaking performance with drastically less infrastructure cost, making On-Ramp wireless an ideal solution for many applications including utility, energy, agriculture, tracking and other M2M applications.
The issue On-Ramp had was finding a partner that offered end-to end wireless networking products to meet all of their needs. They needed a complete wireless networking solution that was made to withstand the rigors of field use with minimal lead time while being competitively priced.
L-com was the perfect partner, able to meet the needs of On-Ramp’s Total Reach Network with a wide range of products that included coaxial adapters, DC surge protectors, 2.4 GHz Wi-Fi antennas and low-loss cable assemblies. With the help of L-com’s products, On-Ramp able to supply its customers with an innovative networking solution with unmatched performance, lower TCO and greater ROI.
To read the full details of this case study, click here.