To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com offers bulk fiber optic cable including singlemode, multimode, Duplex, OM1. OM2, OM3, OM4, 10 & 100 Gigabit, Hi Flex, breakout style and distribution style. Our bulk fiber optic cable is an optimal choice for a variety of applications, including data center connectivity, enterprise networks, industrial automation, military and government applications and telecommunications.

Our Singlemode fiber optic cable is designed for long-distance communication. It has a smaller core diameter than multimode fiber, which allows it to transmit light over longer distances without losing signal strength. Singlemode fiber is typically used for applications such as telecommunications and enterprise networks. The Multimode fiber optic cable is designed for shorter-distance communication. It has a larger core diameter than singlemode fiber, which allows it to transmit light over shorter distances without losing signal strength. Multimode fiber is typically used for applications such as data center connectivity and industrial automation. L-com's Duplex fiber optic cable contains two fibers, one for transmitting data and one for receiving data. This type of cable is typically used for point-to-point communication, such as between two servers in a data center.

Order your bulk fiber optic cable now to receive same business day shipping!