To our valued customers: Please note that our warehouses and offices will be closed on Thursday, July 4th in observance of the holiday.
 
 

L-com features a variety of coax terminators including SMA, BNC, Type-N & Type-F, high performance, fully insulated and 50 Ohm and 75 Ohm line coaxial cable termination. A coax terminator is a device that is used to terminate a coaxial cable. A terminated cable is one that has no signal reflection. This is important for maintaining the integrity of the signal and preventing interference.

There are many different types of coax terminators that L-com offers, each with its own advantages and disadvantages. Some of the most common types include:

  • SMA terminators: SMA terminators are a popular choice for high-frequency applications. They are small and lightweight, making them easy to install.
  • BNC terminators: BNC terminators are another popular choice. They are less expensive than SMA terminators, but they are also larger and heavier.
  • Type-N terminators: Type-N terminators are the most common type of coaxial terminator. They are relatively inexpensive and readily available here.
  • Type-F terminators: Type-F terminators are used with coaxial cables that are used for television and FM radio reception.


The type of coax terminator that you choose will depend on the specific application. For example, if you are using a high-frequency cable for a radio antenna, you will need to use an SMA terminator. If you are using a cable for television reception, you can use a Type-F coaxial terminator.

L-com offers a variety of coax terminators, including SMA, BNC, Type-N, and Type-F. Our terminators are high performance, fully insulated, and 50 Ohm and 75 ohm line coaxial cable termination. They are also available in a variety of sizes and materials to meet the needs of different applications.


L-com is a well-known provider of high-quality coax terminators, and we are accessible by phone, chat, and email. We are a global leader in wired and wireless connectivity products, providing solutions for many major industries, including electronics, medical, industrial automation, military, and telecommunications. We are known for our low or no minimum order quantities and fast response times. Please contact our knowledgeable technical support and sales teams if you have questions about our coax terminators or other components. Order these coax terminators now for same business day shipping!