To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
These handy duplex clips can be used to join two individual SC connectors together to become a duplex assembly. These one piece clips simply snap into place securely connecting the two individual connectors together. These clips can be used on virtually any simplex SC connector and can be removed and re-attached as needed. Call today for discounted volume pricing!