To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
The Sub-Zero enclosures are designed for use in environments down to -30°F (-34°C). It features a thermostat controlled heating system that will along with the heat generated by an internal device such as an access point, maintain a nominal internal ambient temperature of +40°F (4°C).