To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com offers a variety of USB hubs, host controller cards, conversion cables and print servers. Our USB hubs are devices that allow you to connect multiple USB devices to a single USB port. This is useful if you have more USB devices than you have available ports. These USB hubs can be either powered or unpowered. Powered hubs have their own power supply, while unpowered hubs rely on the power from the host device. L-com's Controller cards are add-on cards that can be installed in a computer to add additional USB ports. This is a good option if your computer does not have enough built-in USB ports. Our controller cards can be either internal or external. Internal controller cards are installed inside the computer, while external controller cards connect to the computer via a USB port.

L-com's conversion cables are cables that allow you to connect a USB device to a non-USB port. For example, you can use a USB to serial cable to connect a USB device to a serial port. Our conversion cables can be either active or passive. Active conversion cables have a chip that converts the signal from one type of port to another. Passive conversion cables do not have a chip, so they can only convert signals over short distances. L-com's print servers are devices that allow you to share a printer over a network. This is useful if you have multiple computers in your home or office that need to access the same printer. Our print servers can be either wired or wireless. Wired print servers connect to the network via an Ethernet cable, while wireless print servers connect to the network using Wi-Fi. Order your USB Hubs, Controller Cards, Conversion Cables, Print Servers now to receive same business day shipping!