To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com offers a wide range of USB ferrite cables, including USB 2.0, USB 3.0, and USB 3.0 LSZH cables. These cables feature ferrite beads that help to suppress electromagnetic interference (EMI) from and to a device. EMI can cause problems with data transmission, so the ferrite beads help to ensure that your data is transferred smoothly and without errors. L-com's USB ferrite cables are available in a variety of lengths and connector types. 

Ferrite beads are made of a magnetic material that creates an impedance to high-frequency signals. This impedance helps to block EMI from traveling along the cable. Ferrite beads are also effective at reducing crosstalk between adjacent cables.

L-com's USB ferrite cables are ideal for a variety of applications, including:

  • Connecting computers to peripherals, such as printers, scanners, and external hard drives
  • Charging devices, such as smartphones, tablets, and e-readers
  • Transferring data between devices
  • Connecting to the internet using a USB modem


Here are some of the benefits of using L-com USB ferrite cables:

  • Reduced EMI and crosstalk
  • Improved data transmission reliability
  • Increased cable durability
  • Wide range of lengths and colors to choose from

If you are looking for a high-quality USB cable that can help to reduce EMI and improve data transmission reliability, then L-com USB ferrite cables are a viable option. Order one or more USB Ferrite Cables now to receive same business day shipping!