To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

240V NEMA Enclosures with Euro Style Plugs added to L-com’s Product Portfolio

Thursday, July 23, 2009

NORTH ANDOVER, MA – July 24, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity solutions, today announced the addition of  12 new NEMA rated equipment enclosures with Euro style power plugs.  

This new series of 240 Volt Euro NEMA enclosures comprises myriad options including heaters, cooling fans, vented enclosures as well as ABS plastic or fiberglass construction.

 

 “By offering the new Euro style enclosures, we can offer a host of options to our European customers for protecting both wired and wireless communications equipment. These new units do not require cumbersome plug adapters or converters as the plugs are built right into the enclosures,” said Karl Blomgren, Product Manager.

He further commented on the unique plug configuration, “These robust enclosures were designed to be used in most European countries (such as Germany, Italy, UK, France, Spain and others) because of the “Universal Plug” configuration that accepts most country plug conventions. Thus you can use these NEMA enclosures throughout Europe for consistency and flexibility in all of your applications.”

For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, kblomgren@l-com.com

About L-com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com