To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

Activate Your Workspace with L-com’s New Vertical Wall-Mount Cabinets

Monday, December 9, 2024

Innovative Rack Enclosures Are Space Efficient in 4 Capacities and 5 Depth Ranges

IRVINE, Calif. − L-com, an Infinite Electronics brand and a supplier of wired and wireless connectivity products, has just introduced a line of vertical wall-mount cabinets in either black or white finish. The top-loading enclosures orient electronic components vertically, taking advantage of a room’s or hallway’s unused wall space and allowing low-profile storage of deep equipment.

There are 25 new models in sizes from 2U to 6U and in five adjustable rack depth ranges. They can hold just about anything of the standard 19-inch width, from servers to switches to AV equipment. They have low profiles, with the 2U models sticking out less than 5 inches from a wall and the 6U versions extending less than a foot. This allows them to fit into not only small rooms but IT closets, back offices and even busy hallways and retail spaces.

Both the black and the white models share a set of useful features. They are made of heavy-duty cold-rolled steel and steadily hold 132 pounds of gear. Size options are 2U, 3U, 4U and 6U. Security locks prevent unauthorized access. The rack rails have both M6 and 12-24 threaded mounting options and include a 1U or 2U upper patch panel bracket. Punchouts make cable management easier.

There are 17 new vertical wall-mount cabinets in L-com’s white, electro-static, powder-coated finish. This modern aesthetic will enhance the visual appeal of any installation. It is especially beneficial in environments where the rack is visible or in customer-facing areas. The white cabinets come with adjustable rack rails in five range options: 13 to 16 inches, 17 to 22, 21 to 24, 25 to 28 and 32 to 35.

There are eight new cabinets in the traditional black finish. Their rack rails are adjustable in four range options: 13 to 16 inches, 17 to 22, 21 to 24 and 32 to 35.

L-com’s new vertical wall enclosures ship pre-assembled and with wall anchor bolts and both M6 and 12-24 thread mounting options.

“Vertical wall-mount cabinets are great at allowing you to get the most use out of your workspaces,” said Product Line Manager Tim Houghton. “Their combination of low profile and big depth lets you activate wall space you might not have ever thought of using.”

L-com’s vertical wall-mount cabinets are in stock and available for free same-day shipping. For inquiries, please call +1 (866) 308-2450.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. Headquartered in North Andover, Mass., L-com is ISO 9001:2015-certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Infinite operates a global portfolio of leading in-stock connectivity solution brands. The brands help propel the world’s innovators forward by working urgently to provide products, solutions and real-time support for their customers. Backed by Warburg Pincus, Infinite’s brands serve customers across a wide range of industries with a broad inventory selection, same-day shipping and 24/7 customer service. Learn more at infiniteelectronics.com.

###

Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
+1 (978) 682-6936