NORTH ANDOVER, MA - 03/25/2010 - L-com, Inc., a global leader in the manufacture of wired and wireless connectivity equipment, today announced the availability of a new family of Panel Enclosure Antennas for 2.4GHz, 3.5GHz and 5.1/5.8GHz wireless networks.
These new space-saving Panel Enclosure Antennas are simple to install and are particularly well-suited for tight-space applications. And, in spite of their small form factor, they provide enough internal space for an Access Point or Bridge Card behind the antenna. They also feature weatherproof, quick-connect and -disconnect feed thru jacks, enabling plug in PoE connectivity after installation.
To service the unit, technicians can simply disconnect the CAT5 cable and remove the whole antenna without having to open the radome and unwire the radio from the antenna.
“Antennas and wireless networking equipment are essential in an installation, so it makes sense to put them together, saving on installation costs, space allotments, and repair time,” said Karl Blomgren, L-com Product Manager for Antennas. “We don’t just offer a huge variety of wireless products; we offer smart products, ones that simplify our customers’ lives.”
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/