NORTH ANDOVER, MA – 05/04/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a complete line of 4-20 mA current loop lightning and surge protectors. The new protectors can minimize risks to expensive sensors and process controllers by lightning strikes or power surges. “Current loops are ideal for analog and data transmission because of their inherent insensitivity to electrical noise,” said Patrick Pesa, product manager. “With the introduction of a complete family of 4-20 mA surge protectors at competitive prices, customers need not look further than L-com.” All of the new models are available in 12V, 15V and 24V configurations, and in indoor, outdoor, and industrial grades. Most of them provide three-stage protection using screw terminals. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/ |