NORTH ANDOVER, MA – 2/2/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products is now offering low-loss coax cable assemblies featuring FME (For Mobile Equipment) connectors. These miniature 50Ω RF connectors allow cables to be snaked through tight access holes or spaces. FME connectors are commonly used in cellular communication devices as well as low frequency mobile antenna applications.
"FME connectors are the perfect complement to our already broad coax line," said Patrick Pesa, Product Manager. "They are popular because they have screw-down termination like the SMA connector, but are low-profile to fit through holes. I think our customers will be glad we added them."
These high-quality, fully-tested cable assemblies are built with L-com's CA-195 low-loss coax cable. Standard assemblies include FME to FME and FME to BNC. Along with standard cable assemblies, custom cable assemblies can be configured using the on-line Product Configurator.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, mailto:newsletters@L-com.com
To see all of our press releases, click here.
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/