NORTH ANDOVER, MA – 04/27/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has added secured, keyed, LC adapter sub-panels in multiple colors to its product offering. The new sub-panels can be used to populate L-com’s fiber patch panel enclosures.
“One of the biggest concerns facing mission-critical fiber optic circuits is connection error, whether intentional or accidental,” said Manuel Martinez, product manager. “Addressing this issue is of significant importance to our customers.”
A key feature of these sub-panels is the color-coded keying options. Each color code represents a distinct keying option. Only connectors of the same color can be mated to the corresponding colored receptacle.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/