NORTH ANDOVER, MA – 10/13/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, now carries plastic optical fiber (POF) cable assemblies with the HFBR interface attached. L-com carries simplex and duplex versions, in both latching and non-latching connector types.
HFBR connectors are common in the automotive, industrial control, medical and gaming equipment industries. They are an ideal match for plastic fiber, which is generally more durable than glass fiber and has a much larger core size making it easier to terminate and providing more bandwidth over short distances. “We found the HFBR interface difficult to acquire in our industry,” said Steve Smith, L-com’s product manager in charge of fiber optic products, “but it is an important interface for many products and services. Providing HFBR cables makes our product line that much more complete.” Along with the off-the-shelf lengths, L-com will be manufacturing custom lengths of these cables with short lead times. | |
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.