High-flex USB 2.0 cables maintain connectivity through extreme bend cycle counts NORTH ANDOVER, MA – September 29, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has released high-flex versions of its type A-A and type A-B USB 2.0 cables. The new cables are rated for a minimum of 10,000 bend cycles. “We’re working to expand the use of USB cabling to applications it normally wouldn’t work in,” said Steve Smith, product manager. “High-flex applications absolutely require this kind of cable.” Standard USB 2.0 cables fail at approximately 1,000 bend cycles. The special bulk cable used in these new assemblies has a polyurethane jacket and high strand-count data and power conductors. The new cables will be available in lengths ranging from 0.5 to 5 meters. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/. |