To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Addresses Legacy Industrial Networking Applications with RS-232 Interface Converters

Tuesday, October 26, 2010

NORTH ANDOVER, MA – 10/27/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, has developed a line of RS-232 interface converters to address legacy industrial networking applications.

"We can now offer our own brand of RS-232 interface converters that provide the same, or in some cases better, feature sets at lower list prices than our competitors," said Peter McNeil, Product Manager.

The new SC-232 line features both port-powered and externally powered models as well as an opto-isolation option on some models. Each RS-232 interface converter ships with a DB9-to-screw terminal block adapter and is covered by L-com’s standard one-year warranty.

The new SC-232 line is in stock and ready to ship.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.