L-com Adds 2-Port Gigabit 49VDC PoE Injector/Midspan with Integral Power Supply NORTH ANDOVER, MA - 06/13/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added a new 2-Port Gigabit Power-Over-Ethernet (PoE) DC Injector/Midspan, the PS4834GB-POE-2. This new PoE device provides 48VDC @ 33.5W of power to each of its two ports via its internal power supply. Built in protection circuits help prevent damage to equipment attached. IEEE 802.3af/at compatible, they can work on any 10/100/1000 Mbps networks. These units have keyhole slots in the rear for wall-mounting, and the expandable slide/groove design allows multiple units to be fastened together by sliding one into the grooves on the side of another. This feature provides extra flexibility as the system grows and additional capacity is needed. The list price is under $50US, making them an affordable way to future-proof electronics installations. "As PoE adoption grows, so does the need for flexibility to meet the changing demands of the technology," said Patrick Pesa, Director of Product Development. "In the past twelve months we've introduced all-in-one midspans and splitter/taps with adjustable DC outputs, and these new products continue those efforts to enhance the flexibility of PoE." These items should be available to ship starting June 21 from L-com's HyperLink distribution center in Boca Raton, FL, USA. Detailed diagrams, 2D engineering drawings, and datasheets are available on L-com's website. For high-res versions of the images suitable for print publication, follow these links, right click on each image, and select Save As: https://www.l-com.com/lcom_emails/2013/061313/PS4834GB_POE_2.jpg https://www.l-com.com/lcom_emails/2013/061313/PS4834GB_POE_2_pmi_2.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |