NORTH ANDOVER, MA – 5/25/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today that fully shielded versions of its popular IP67 rated USB revision 2.0 cables are now available.
"The USB interface—originally intended to connect peripheral devices to desktop PCs—is now being used in almost all network settings, from high-speed data centers to industrial applications and outdoor networks" said Steve Smith, L-com Product Manager for USB products.
"Many customers contacted us to say that in dirty, wet environments they were using rough workarounds to ground the USB shield in our existing IP67 USB cables. We realized that our customers needed an alternative, so we came up with these cables that ground right to a panel. This is another example of L-com listening to what our customers had to say and using it to drive innovation."
Cable options are:
1. | A die cast steel, panel mountable female USB A connector to a standard male USB A connector (WPUSBAXSH series). The steel housing allows for efficient grounding to a panel or enclosure | ![]() |
2. | A male USB A connector with a metal coupling nut to a standard male USB B connector (WPUSBABSH series). | ![]() |
When mated together these cables provide a completely shielded IP67 solution. Use the cover, WPCVR-SHLD-USB, to seal the female USB port when not in use. | ![]() |
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/