L-com Adds New DB15 Male and Female Shielded Connector Covers
![]()
NORTH ANDOVER, MA - 03/27/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that it will now be offering DB15 male and female metal shielded connector covers. These covers are inexpensive and are perfect for protecting unused DB15 ports, cables or any equipment from physical damage, dirt, and dust. Unlike plastic covers, these metal covers also maintain protection against EMI/RFI.
"L-com has sold several thousand of the existing DB9 and DB25 shielded covers so launching the DB15 version was long overdue," said Steve Smith, Product Manager.
The DB15 covers feature 4-40 threaded screws so they can lock tightly to mating connectors and are available to cover either male or female connectors. Shielded connector covers like these are most commonly used in applications such as serial data transmission, data networks, instrument control, and device management.
L-com offers a full selection of D-Sub connector covers. Large quantity pricing is also available.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/
###