L-com Adds New Right Angle RCA and TS 1/4" Audio/Video Adapters ![]() NORTH ANDOVER, MA - 01/18/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has introduced two new audio/video adapters that allow tight right angles at ports. The new RCA and TS 1/4" adapters have rugged molded construction for demanding environments and have gold plated contacts to ensure superior audio transmission. RCA connectors are commonly used in audio applications and are used in component and composite analog video connections. The TS 1/4" connector type is used in many high definition and professional audio applications. In both cases, plugging a straight cable into a jack at a tight angle will cause stress and damage to both the cable and the port. These new male/female adapters solve this problem by providing a controlled 90 degree angle. "We've recently added right angle adapters for D-Subminiature, USB, RJ45, and other connectors," said Steve Smith, Product Manager. "These are the first right angle adapters for these two popular ports and we expect them to be very helpful in the audio industry." The new adapters are scheduled to be stocked in the USA by March, allowing same-day shipment on orders. Detailed engineering drawings and 3D CAD models are available for free on L-com's website. For a high-res version of the image suitable for print publication, follow this link, right click on the image, and select Save As: https://www.l-com.com/lcom_emails/2013/011813/ra_rcamf.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, mailto:dfallon@l-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |