L-com Adds New Right Angle USB Cables to Address Confined Space Applications ![]() NORTH ANDOVER, MA - 12/7/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has expanded its line of right angle USB cable assemblies to address confined and tight space USB connectivity applications. L-com has added 18 new configurations to its highly successful right angle USB cable series. These new angled USB 2.0 cable assemblies feature every right angle combination off-the-shelf. L-com's specialized USB cables solve difficult connection issues in tight places. Each cable assembly is constructed with USB 2.0 compliant cable with 26 AWG power leads and feature 30 micro-inch gold plated contacts which provide reliable connections even with repeated mating cycles. Additionally, eight lengths are available for each series ranging from 0.3 meters to 5 meters. "We have seen great success with the initial release of our right angle USB series," said Steve Smith, Product Manager. "We were seeing more requests coming in for different right angle combinations that became custom cable orders. By adding these additional new configurations to our stock product offering, we can provide faster delivery and easier ordering for our customers." The angled USB cables are now available for shipment and can be ordered directly from L-com or from L-com's authorized distributors. A .pdf tip explaining the different right angle combinations is available for free download from L-com's website. For a high resolution version of the image suitable for print publication, click here: https://www.l-com.com/lcom_emails/2012/120712/ca90la_90lb_m.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |