L-com Adds New USB3 Vision Cables with Thumbscrew Hardware
![]()
NORTH ANDOVER, MA -1/09/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that it has engineered three new USB 3.0 cables equipped with thumbscrews for use with USB3 Vision standard applications. These cables are built precisely to the USB3 Vision specification hosted by the AIA (Automated Imaging Association) for the machine vision industry.
"In addition to supporting cabling for the machine vision camera market, I expect these products to be designed into many other applications where the lockdown thumbscrew hardware provides a secure connection every time," said Steve Smith, Product Manager. "One drawback to USB connections is that the friction fit connectors can become disconnected by vibration and jostling."
![]()
In addition to applications where the secure thumbscrew is beneficial, L-com's USB3 Vision Cables can also be used for data storage, data acquisition, and video transfer. These USB cables are available in three versions, Type Micro B with Thumbscrews to Standard Type A, Type B with Thumbscrews to Standard Type A, and Type A with Thumbscrews to Standard Type A. All three configurations are available in a variety of off the shelf lengths including 0.3, 0.5, 1, 2, 3 or 5 meters.
L-com's USB3 Vision Cables can be ordered directly from the L-com.com web site or by calling L-com sales at 1-800-341-5266.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/
###