L-com Adds Seven New Wireless Active Products from Planet Networking & Communications ![]() NORTH ANDOVER, MA - 07/03/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added seven new products from Planet Networking & Communications for wireless bridging, range extending, and WLAN access. The new products are intuitive, feature packed, easy to use and very competitively priced. Planet's WNAP-6305 offers high power outdoor wireless access, with 600mW power through a 2.4 GHz 12dBi built-in antenna or through an optional add-on antenna. The WNAP-6306 adds more flexibility with a built-in N-type antenna connector for directly attaching to various types of antennas. The WNAP-6350 and WNAP-7350 are 2.4 GHz and 5 GHz (respectively) outdoor access points with very high data rates and adjustable power outputs. The WNAP-1260 is a wall plug universal WiFi repeater can provide up to 300Mbps wireless network sharing while using a convenient, compact design for nearly any location. The WDRT-731U intelligently breaks wireless signals between 5 GHz for watching HD videos or playing online games, and 2.4 GHz for surfing the Internet. Finally, the WNAP-C3220 is a stylish PoE wireless access point offering up to 300Mbps 802.11n wireless speed, multiple operation modes and Gigabit LAN connectivity. "Planet is very aggressive in offering new products and keeping ahead of the technology curve," said Patrick Pesa, Director of Product Development. "We will be evaluating these products as they become available and making them available to our customers." The new Planet products join a wide range of high-quality wireless devices from brands such as EnGenius, Ubiquiti, Linksys and Netgear. All of the parts have free downloadable content on L-com's website. For a high-res version of the image suitable for print publication, please follow this link, right click on the image and select Save As: https://www.l-com.com/lcom_emails/2013/070313/WNAP_6350.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |