To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Adds USB Micro B and Black A-B Cable Assemblies

Wednesday, August 4, 2010

NORTH ANDOVER, MA – 8/5/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, announced today that it has added two new USB 2.0 product families to its product offering. The first is a USB type A to USB micro B series of cable assemblies, and the second is a black version of the company's best selling CSMUAB-xM cables.

The USB micro B-type connectors are gaining popularity because of their small form-factor. Common applications for this connector include cell phones and PDA’s. 

The new black USB cables, CAUBLKAB-xM, feature USB 2.0 compliant speeds of up to 480 Mbps and 20 AWG power conductors for maximum power transfer from host to peripheral.  For years, gray has always been the preferred color for computer cabling equipment.  But today, black is used in an equal number of applications.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.