To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com announces a new HyperLink Brand 2.4 GHz 27 dBi Grid Antenna

Monday, June 16, 2008

North Andover, MA – June 17, 2008 – L-com Global Connectivity, renowned manufacturer and distributor of HyperLink brand antennas, amplifiers, waterproof enclosures, and other wireless connection equipment, announced their new 2.4 GHz 27 dBi Grid Antenna.

The HyperGain HG2427G high-performance reflector grid Wi-Fi Antenna provides 26.5 dBi gain for long-range highly directional applications. This includes point to point systems, point to multi-point and wireless bridges in the 2.4 GHz ISM band as well as IEEE 802.11b and 802.11g. It can be installed for either vertical or horizontal polarization.

This 27dBi grid antenna's construction features a die cast aluminum reflector grid for superior strength and light weight. The antenna's 4-piece reflector grid is simple to assemble and significantly reduces shipping costs.

The HG2427G compliments the successful family of grid antennas that include the popular HG2424G and HG2430G models, offering customers the option to select the antenna that best fits their network and communication requirements.

Orders for the HG2427G can be taken now, with expected delivery by mid-August 2008.

For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, mailto:kblomgren@hyperlinktech.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com