North Andover, MA, -- In addition to L-com's already extensive harsh-environment, waterproof, and industrial IP67 line of cables, connectors, and adapters, L-com will now be carrying a line of fiber optic and Category 5e Ethernet cable assemblies that come pre-terminated with IP67 water seal grommets at either end.
The new FODLCG and TRD855WTG cable product lines, which come in various lengths, are perfect off-the-shelf solutions for allowing cables to pass through openings but keeping water out. L-com is now manufacturing and stocking these cables domestically in order to offer same-day shipping.
The grommets are also available for making custom cable assemblies. L-com will distribute these sealing grommets with no minimum order quantity required, so they are perfect for electrical or design engineers who may be prototyping and specifying new products. The product is set to retail for under $100. Along with the off-the-shelf enclosure product that L-com stocks for same-day shipments, L-com announced that other options, such as heated and cooled units, 220 VAC, 12 VDC, and Power-over-Ethernet (POE) models would be available by request.
For further information, please contact Mr. David Fallon or visit https://www.L-com.com.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
- Assembled and Injection Molded Data Cables
- Fiber Optic Cable Assemblies and Adapters
- Modular and Telco Assemblies
- Low Loss Video and Monitor Cables
- Unique Bulkhead Connectors
- Machined or Cast Coaxial Connectors and Adapters
- Sheet Metal Fabrication of Rack Panels and Enclosures
- Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
- Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit https://www.L-com.com
------------------------------------------------------------------------------------
L-com Connectivity Products 45 Beechwood Drive North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com Phone: 1-800-341-5266 Fax: 1-978-689-9484