L-com Announces New Industrial Ethernet Switches for Harsh Environments NORTH ANDOVER, MA – 10/14/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today that they will now offer their own line of industrial Ethernet switches to address the growing industrial networking market. The L-com IES (Industrial Ethernet Switch) switch line features DIN rail mounting, dual 24V DC power inputs, rugged aluminum cases, and an operating temperature of -40°C to +70°C. The IES Series switches are plug-and-play, unmanaged devices and can be installed in minutes providing seamless connectivity to IP-enabled devices such as PLCs, drives, motors, pumps, and meters. “Now we are truly able to offer our customers a complete industrial Ethernet solution with the addition of the IES series switches,” said Peter McNeil, Ethernet Product Manager. “L-com now carries all the components required to build an industrial Ethernet network ranging from shielded category rated cabling, fiber optic cables, DIN rail, NEMA enclosures and now the IES Series Switches.” L-com offers several models to choose from including copper only or combination fiber optic and copper interfaces. Fiber versions are offered in both multimode (2km) and single mode options up to 80km. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |