NORTH ANDOVER, Mass., March 9, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity solutions has introduced a new Digital Signage distribution system to address the growing market for digital signage solutions. "Increasingly we have had requests for more versatile, scalable digital signage systems from our customers. Due to this demand we have developed this easy to use solution which grows with the customers business," said Greg Pepin Product Manager.
The new SignDriver™ system consists of a 4 port hub which connects via CAT-X cabling to remote units. Options for this line include audio support as well as several off the shelf kits that include a single distribution hub and one remote unit (with audio and without). The SignDriver™ system can extend a maximum of 1,000 feet away from the source and supports video resolutions of up to 1600x1280@60hz.
For more information about this release, please contact:
Greg Pepin, Product Manager
978-682-6936 x1186, gpepin@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com