North Andover, MA -- L-com Connectivity Products announces the availability of its new CMP24 series of plenum rated IEEE-488 cable assemblies.
These cables utilize a CMP rated cable jacket and overmold material. CMP rated material is a fire retardent compound that possesses exceptional self-extinguishing characteristics. Plenum rated cables are necessary when the highest fire resistant assemblies are required. Cable construction features foil/braid shield, 12 FEP insulated 26 AWG twisted pairs, and standard IEEE-488 male/female connectors. A unique stamped steel internal enclosure provides 100 percent shielding and a robust strain relief.
L-com will manufacture custom plenum rated IEEE-488 cable assemblies with modest minimum requirements.
For further information, please contact Mr. Steve Smith or visit https://www.L-com.com.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
- Assembled and Injection Molded Data Cables
- Fiber Optic Cable Assemblies and Adapters
- Modular and Telco Assemblies
- Low Loss Video and Monitor Cables
- Unique Bulkhead Connectors
- Machined or Cast Coaxial Connectors and Adapters
- Sheet Metal Fabrication of Rack Panels and Enclosures
- Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
- Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit https://www.L-com.com.
Contact:
Steve Smith
Product Manager
L-com, Inc.
978-682-6936 x156
ssmith@L-com.com
45 Beechwood Drive
North Andover, MA, 01845
https://www.L-com.com