North Andover, MA – February 17, 2009 – L-com Global Connectivity today announced the addition of several new products using the DB15 interface.
![]()
The new products, including two right-angle DB15 adapters, and new male to male and male to female premium D-Sub cables, are being stocked at L-com's North Andover fulfillment center for same-day shipment.
The new right angle adapters are perfect for applications that require cables to be connected in tight spaces. They come in either "exit 1" or "exit 2" styles so the cable can approach from either direction.
The new premium D-Sub DB15 assemblies feature double shielded cable (foil + braid) and are designed to solve data transmission problems where high levels of EMI/RFI are present.
The new products will complement the already extensive line of DB15 products including the popular "field termination" connector.
For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. https://www.L-com.com/