L-com Announces the Availability of the Planet FT-807 Plastic Optical Fiber (POF) SMI Media Converter
L-com Announces the Availability of the Planet FT-807 Plastic Optical Fiber (POF) SMI Media Converter
Wednesday, April 19, 2006
North Andover, MA, -- L-com Connectivity Products has recently added the Planet FT-807 10/100TX to 100FX POF SMI media converter to its active equipment line up. This economical yet robust media converter converts Cat5E/Cat6 to POF via the popular SMI type connector. The SMI (small multimedia interface) port is designed for use with plastic fiber optic cables with a diameter of 1.0mm. POF offers a low-cost, high-speed data transmission solution, which is also immune to RFI and EMI. The SMI interface meets the IEEE 1394b specification and can transmit data up to 50 meters.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
Assembled and Injection Molded Data Cables
Fiber Optic Cable Assemblies and Adapters
Modular and Telco Assemblies
Low Loss Video and Monitor Cables
Unique Bulkhead Connectors
Machined or Cast Coaxial Connectors and Adapters
Sheet Metal Fabrication of Rack Panels and Enclosures
Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit https://www.L-com.com