North Andover, MA -- L-com Connectivity Products has announced the availability of its new ECF504-5M panel mountable USB shielded coupler assembly.
![]()
This addition to the popular USB panel mount adapter line allows the user the flexibility to configure their own assembly. It features a shielded bulkhead Type A Jack with 5 meters of un-terminated USB 2.0 compliant cable. The user can cut the cable to the desired length and hard wire or terminate it with their connector of choice. Utilizing a unique mounting flange these units are usable in virtually any panel thickness and provide a cost effective way to feed a USB bus through a panel or enclosure.
L-com can custom terminate these cable ends with modest minimum requirements.
Outer housing is UL94V0 rated ABS with a metallic conductive plating that maintains shielding integrity. All contact surfaces feature 30 microinch gold plating.
For further information, please contact Mr. Steve Smith or visit https://www.L-com.com.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
- Assembled and Injection Molded Data Cables
- Fiber Optic Cable Assemblies and Adapters
- Modular and Telco Assemblies
- Low Loss Video and Monitor Cables
- Unique Bulkhead Connectors
- Machined or Cast Coaxial Connectors and Adapters
- Sheet Metal Fabrication of Rack Panels and Enclosures
- Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
- Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit https://www.L-com.com.
Contact:
Steve Smith
Product Manager
L-com, Inc.
978-682-6936 x156
ssmith@L-com.com
45 Beechwood Drive
North Andover, MA, 01845
https://www.L-com.com