L-com brand DIN rail-mountable fiber media converters operate up to 80km NORTH ANDOVER, MA – 08/31/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has released a new line of industrial media converters that are DIN rail-mountable and can support up to 80-kilometer transmission distances over single mode cable. “With the growth of industrial networks, we have seen an increased need from our customers for cost-effective, easy-to-install, rugged, industrial connectivity solutions,” said Peter McNeil, product manager. “Our new line of DIN rail industrial media converters addresses these needs.” Media converters are used to extend Ethernet LANs over fiber optic cabling. L-com’s new industrial media converters are available in four Single Mode versions (up to 20km, 40km, 60km and 80km) and a Multimode version (up to 2km). For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |