L-com branded CPE wireless access points offer dependability and security NORTH ANDOVER, MA – October 5, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries two L-com branded customer-premises equipment (CPE) wireless access points. The new units are weatherproof, offering years of trouble-free service; and secure, featuring WPA, WPA2, WPA-PSK, 802.1x as well as other security protocols. “We’re pleased to offer these CPE units at terrific price points,” said Patrick Pesa, director of product development. “They offer great flexibility and reduced inventory stock as they can perform all that is required for establishing reliable wireless networks.” The two new models include a 2.4 GHz IEEE 802.11b/g/n compliant version and a 5.8 GHz IEEE 802.11a/n compliant version, both priced below $100 each. Both units have access point, wireless client, bridge, and repeater operating modes available. They are also both power-over-ethernet ready and come with a PoE injector and power supply. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |