North Andover, MA · July 24, 2008 -- L-com Connectivity Products has just released a new series of Latching Serial ATA (SATA) cable assemblies that provide secure connections. Serial ATA cables are replacing wide Parallel ATA ribbon cables in many applications. The Serial ATA cable is smaller, more flexible and therefore easier to route inside a chassis. With the trend toward miniaturization, these characteristics are beneficial in many product designs. These cable assemblies feature two shielded 26 AWG pairs in a PVC jacket, and gold plated contacts. Two versions are offered, one with a straight to straight connector configuration and the other with a straight to right angle connector configuration. In addition to six standard off the shelf lengths, L-com can manufacture custom lengths to meet your specific design requirements.
![]()
![]()
For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x156, ssmith@L-com.com
About L-com
Founded in 1982, L-com (www.L-com.com) is a privately held Massachusetts Corporation dedicated to the design and production of a wide range of interconnect products for the electronics and data communications industries. Primary product emphasis is placed on copper and fiber cable assemblies and accessories for modular and coaxial applications as well as computer networking. The company endeavors to serve the industry by offering solutions to interconnect problems. This effort has led to the development of many new products, some of which are proprietary. L-com has also introduced switching and testing devices in each of their basic product areas. Products are marketed domestically and internationally.