NORTH ANDOVER, Mass. (July 21, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a 4G/LTE mobile booster kit.
L-com's HAKIT-72150-M01 4G/LTE mobile booster kit is an ideal solution to meet today's ever-increasing need for consistent cellular connectivity for mobile devices. It can be difficult to obtain a reliable cellular signal while in a car, RV or boat. This booster captures weak cellular signals and transfers them to a cell booster. The cell booster then amplifies and rebroadcasts the signals inside the vehicle, improving call quality and increasing data speeds while reducing the frequency of dropped calls.
"Weak signal areas as well as physical obstructions inside a vehicle can affect the performance of cellular devices. When installed in a vehicle, our new 4G/LTE mobile booster kit helps improve cellular voice and data signals so users can enjoy crystal-clear calls and fast, consistent data speeds," said Ken Burgner, Product Manager.
The HAKIT-72150-M01 mobile booster kit mounts inside almost any vehicle and can be especially useful for commercial vehicles used for utility, construction, public safety (fire and police) and transportation (taxi, bus, etc.). Designed for in-vehicle use only, it is powered by a 12V power adapter which is included. This mobile booster kit allows you to simultaneously connect multiple mobile devices and works with 2G, 3G and 4G networks on most US carriers. The boosted cellular signal also helps reduce radiation and increase battery life for up to 2 hours of additional talk time in weak-signal areas.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/