To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Debuts New High Flex HDMI Cable Assemblies

Monday, August 28, 2017

NORTH ANDOVER, Mass. (August, 29 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new series of high-flex HDMI cables to address confined space A/V applications.

L-com’s high flex HDMI cables were designed to address applications where routing an HDMI cable through tight spaces and around tight corners is required. Additionally, these new high flex HDMI cables can be used in applications where the cable is frequently moved or flexed.

The new VHA00001 series cables feature a fully molded back shell construction providing excellent strain relief and 30 micro-inch gold plated contacts which minimize signal loss even after repeated mating cycles. Additionally, these cables support 4K and 1080p resolutions.

 “We are excited to offer these new high flex HDMI cables to help our customers with tricky installations where standard cables won’t cut it. In addition to their high flex capabilities, these cables also offer all of the same features found in standard high speed HDMI cables,” said Brian Gates, Product Manager.

L-com’s new high flex HDMI cables are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: