To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Debuts New Short Length, High-Flex Cat5e Cable Assemblies for use in Confined Space Applications

Friday, May 7, 2021

L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of short length, high-flex Cat5e Ethernet cables for use in cramped, confined space applications.

L-com’s short, flex Cat 5e cables assemblies feature a high bend radius that is able to be routed in small spaces without loss of performance. These new Ethernet cable assemblies are available in 15cm to 10m lengths and feature SF/UTP double-shielded TPU jackets with RJ45 connectors. Each assembly has been fluke tested to channel standards and are wired to the TIA 568B.

L-com’s new short, high-flex cable assemblies are perfect for use in tight spaces and are designed to bend or be routed at tighter angles than standard cables. These cables can be used in myriad applications including data centers, Enterprise networks, industrial networks and in any application where space is an issue.

"These new cables were specifically designed to address Ethernet connectivity applications where cables need to be installed in tight areas where sharp angles are required. Many times, connections in panels, enclosures and on DIN rails are very close to each other and using standard cables would impact performance since they exceed their specified bend radius," said Dustin Guttadauro, Product Manager.

L-com’s new short length, high-flex Cat5e cable assemblies are in-stock and available for same-day shipping.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves & Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936