To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Debuts Passive DWDM Mux and Demux Cassettes and 19” Rack-Mount Units

Thursday, April 15, 2021

L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of Dense Wave-Division Multiplexing (DWDM) Mux, Demux and Mux/Demux products to address growing metro and regional transport, PON, GPON and FTTx applications.

L-com’s 20 new DWDM Mux and Demux products consist of both LGX cassettes and 19” rack-mount units that were designed to maximize fiber usage by reducing the fiber count from the central office/head-end and to increase bandwidth between switches, routers and other equipment without requiring additional investment in fiber infrastructure.

The PDW1 series LGX plug-in units feature 4 and 8 channel options, 100 GHz spacing, LC connectors with a UPC polish as well as express channel and 1% optical power monitor ports. The PDW3 models feature a 19” rack-mount design with a space saving 1U height. These units provide two fiber, combo mux/demux operation with 20 channels, 100 GHz spacing, LC UPC connectors and 1% monitor ports in addition to express channel capability. These new DWDM mux/demux products offer industry standard wavelength configurations and are designed for use in inside plant (ISP) applications.

“Our new lineup of passive DWDM mux/demux products allows our customers to save money and valuable space by greatly reducing the number of fibers required to connect sites and equipment in their networks. One big benefit of using DWDM technology is that it increases bandwidth by allowing multiple data streams to be sent simultaneously over a single fiber,” said Paul Hospodar, Product Line Manager.

L-com’s new Passive DWDM Mux and Demux products are in-stock and available for same-day shipping.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves & Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936