NORTH ANDOVER, Mass. (November 22, 2016) -L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new series of premium M12 cable assemblies.
L-com’s new line of premium M12 cable assemblies are made for the toughest, most demanding applications. For extra strength, these cables are built with high-flex, outdoor CMX-rated, double-shielded, FR-TPE cable and IP68 rated M12 connectors. They are designed to exceed category standards and ensure optimal network throughput even in harsh industrial or extreme weather conditions. These cable assemblies are available off-the-shelf with connector options that include D-coded, 4-position male M12, 4-position female M12 and standard RJ45 combinations.
The Flame-Retardant Thermoplastic Elastomer (FR-TPE) cable jackets are resistant to oil, sunlight (UV) and weld spatter. Additionally, these cables are rated for 600V and are flex-tested to 1 million cycles at 10x cable OD and 10 million cycles at 20x cable OD. A double-shielded braid and foil design provides maximum protection from EMI/RFI. These cables are ideal for various applications such as industrial Ethernet, test equipment, industrial controls, factory automation, I/O connectivity and sensor and actuator connectivity.
“Our premium M12 cable assemblies are as robust as they come. They are specifically designed to withstand the harshest conditions and ensure that your network will run smoothly in any harsh environment,” said Dustin Guttadauro, Product Manager.
L-com's premium M12 cables are available in 0.5, 1, 2, 3, 5 and 10 meter lengths. Custom lengths and labeling are also available by contacting L-com or using L-com’s Custom Cable Configurator.
For more information about this release, please contact:
Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/