NORTH ANDOVER, MA – 12/2/10 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, has designed a simple adapter for the USB 2.0 micro B interface, popular on cell phones and PDAs. The new device will adapt from a standard USB type B male connector to a micro B male connector, giving the user the flexibility to use traditional A-B cables on micro B-enabled devices.
L-com already has an extensive line of USB adapters, mixing everything from standard Type A and Type B connectors, male and female, and even right-angle and USB 3.0 adapters. This new adapter is the fourth micro B USB adapter that L-com has introduced.
“The micro B USB connector has made a significant dent in the mini B 5 connectors market," said Steve Smith, Product Manager, “because of its latching design and even smaller form factor. This latest micro B adapter rounds out our product offering, allowing us to adapt pretty much any USB interface to a micro B.”
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.