NORTH ANDOVER, MA, -- June 17, 2009 -- L-com, a global leader in the manufacture of wired and wireless connectivity solutions, has developed a 1U 19” patch panel with four Category 5E/6 Ethernet surge protector modules to protect telecommunications equipment.
The RMSP-CAT6-4 employs ultra-low capacitance semiconductors ensuring superior high frequency response and improved return loss for the four data pairs on each line under surge protection. The easily replaceable modules allow easy field repair in the event of a catastrophic surge event.
The unit is 802.3af Power over Ethernet (PoE) compatible for normal or reverse polarity systems and can be used with 10/100/1000 attached devices such as switches, routers, access points, IP surveillance cameras, and IP phones.
The RMSP-CAT6-4 is in stock and ready for same day shipping.
![]()
For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, mailto:kblomgren@hyperlinktech.com
About L-com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com