NORTH ANDOVER, MA – 1/5/2011 – L-com, Inc., a global leader in the manufacture of wired
and wireless connectivity products, announced today that it has split its USB A-A cable line into two groups, deluxe and premium versions. The move allows L-com to offer varying grades of USB cables to its customers at competitive prices.
“By offering these two versions of our USB 2.0 A-A cable products, we give our customer pricing options that are dependent on their specific applications needs,” said Steve Smith, L-com product manager.
The premium grade USB cables use 20 AWG power conductors and have a light gray jacket, while the deluxe grade uses 26 AWG power conductors and has a standard gray jacket.
Both grades of A-A USB 2.0 cables will be stocked in North Andover, MA for same-day shipment. What is USB-A? Check out our USB A pinout to get more details on Universal Serial Bus, Type-A configurations.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/