NORTH ANDOVER, MA – 9/22/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, has developed new DB15 male to male and male to female cable assemblies with black low-smoke zero-halogen (LSZH) jackets. The new cables join L-com’s existing DB25 and DB9 cables with LSZH jackets.
All LSZH jacketed cables are ideal for military and military-subcontracting customers because they significantly reduce the amount of toxic gases emitted during combustion when compared with standard PVC jackets. This is essential for confined areas like aircraft, submarines and shipboard.
“The men and women of our military absolutely require—and benefit from--LSZH jacketed cables,” said Steve Smith, L-com’s product manager in charge of D-sub products. “To use PVC in an enclosed space is unthinkable. I’m glad L-com is able to support our military’s efforts with quality-built LSZH D-subminiature products.”
All of L-com’s LSZH D-sub cables have 24AWG conductors, allowing users to send more current down the cables, as opposed to their standard D-sub cables (CSM, CSMN, and CS2N), which have 26AWG conductors.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.