To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Expands MPO Fiber Cable Product Line with OM4 and OM3 24 Channel Assemblies

Monday, June 25, 2018

NORTH ANDOVER, Mass. (June 26, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of fiber optic cable assemblies with MPO-style connectors designed for use in high speed data centers, server farms and Enterprise networks.

L-com’s new OM4 and OM3, 24 channel, MPO fiber cables handle network throughput up to 100Gpbs (OM4) per fiber channel while offering up to 24 times the density when compared to a single SC fiber connector. Additional features include low-smoke zero-halogen (LSZH) cable jackets as well as full compatibility with US Conec MTP products.

Additionally, L-com has added new shorter lengths of its popular 6 and 12 channel  OM1,OM2,OM3,OM4 and Single mode fiber cables to address data center and server connectivity applications where shorter cable lengths are required. These new shorter length cables are in stock and are available for immediate delivery.

Another new addition to L-com’s MPO fiber cable line is the FOL-MPO which is a 12 channel, OM3 loop-back cable that provides an economical solution for a number of fiber optic test applications including QFSP. It features a generous yet manageable fiber loop, virtually eliminating bend loss.

 “As today’s networks require higher speeds and closet space is at a premium, in many cases, we are starting to see more of our customers employing MPO interconnects in the data center to address the requirements of small connector size and high speed voice, video and data support,” said Dustin Guttadauro, Product Manager.

L-com’s new MPO fiber products are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: